Added to cart
Added to cart
Go to shopping cart

FIRESTOP SOLUTIONS FOR BOLOGNA CENTRAL STATION, ITALY

Firestopping high-speed train lines 23 meters below ground

Hilti jobsite reference Bologna Central Station Italy

THE CHALLENGE

Hilti jobsite reference Bologna Central Station Italy

Bologna’s Central Station has undergone major changes for line improvement. At the heart of the project is a station for new high-speed lines, located 23 m below ground.

The challenge was to find very reliable fire protection safety systems for such a crowded area.

OUR HILTI SOLUTION

The Astaldi Group, which was overseeing the construction of the station, chose us at Hilti as their firestop partner.

A wide range of our Hilti firestop products were used for the build:

  • To seal openings with a combination of duct runs – Hilti CFS-CT B boards
  • For combustible pipes – Hilti CFS-C collar (which has also been tested for post-earthquake fires) and Hilti CFS-C EL endless collar for standard applications and challenging applications with elbow unions or inclined pipes.
  • For electric cable channels – Hilti CFS-CU cushions

ASK AN ENGINEER

CONTACT US
CONTACT US