Added to cart
Added to cart
Go to shopping cart

HOW HILTI HELPS YOU TO REDUCE CORROSION RISK IN BUILDINGS

Corrosion resistant design for support and fastening systems

Natural gas processing plant

Corrosion matters. It can make structures unsafe and unstable. It can also lead to components and whole installations needing to be replaced. All of which can be costly in money, time and with a risk of real injury. So what can you do?

HOW TO CHOOSE THE RIGHT CORROSION PROTECTION

Where are you building? That’s the key question for corrosion protection. What environment, what climate are you working in, and what material are you fastening into?

Corrosion takes different forms in different environments. So for your own build, you need to consider these factors which can increase the risk of corrosion:

  • Humidity
    Humidity needs to be present for any atmospheric reaction.
  • Temperature
    The higher the temperature, the higher the rate of corrosion will be.
  • Salt
    This can be air containing salt near a coast, or salt from de-icing salt in the winter.
  • Industrial pollution
    High levels of sulfur dioxide speed up corrosive reactions.
  • Galvanic (contact) corrosion
    Caused by two dissimilar materials coming into contact.

Some environments, such as indoor swimming pools, tunnels or chemical plants will need special consideration, and our local Hilti engineers are always happy to give you technical advice.

ASK AN ENGINEER

Corrosion protection and environment

WHAT IS CORROSION PROTECTION

Corrosion is caused when there’s a physical chemical reaction between metal and the environment around it. Corrosion changes the metal’s properties, making it much weaker.

Corrosion can also damage the installation system as well as the metal component and its protection. This can leave the entire installation unsafe and needing to be replaced.

There are two types of corrosion protection to help you increase the life expectancy of metal components you use onsite. These are active and passive corrosion protection.

Active corrosion protection directly influences a corrosive reaction by either using resistant materials, a galvanic separation or cathodic protection.

Passive corrosion protection stops or slows down corrosion by separating metal from a corrosive agent. This is achieved by applying metallic or non-metallic protective layers of coating.

On real jobsites, corrosion resistance is one of the most underestimated aspects when it comes to fastening products. Knowing the basic facts can help the customer to find a suitable and sustainable solution.


Download the complete corrosion brochure

WHAT HILTI DOES TO STOP CORROSION

Our local Hilti engineers are here to help you and can come on site to see first hand what might work best for your build. We also make and design a full range of corrosion protection.

  • Hilti corrosion testing centers
    1 / 7
    Hilti corrosion testing centers

    Our corrosion protection products are tough. They’re all rigorously tested, in exactly the same conditions that you build in. Our products aren’t just tested in a lab, they’re left for months outside in the cold, in tropics, in salty areas, industrial plants and even at sea. So we know they work. Slide through and see more pictures of external and internal testing at Hilti.

  • Hilti corrosion testing center Sweden
    2 / 7
    Sweden

    cold climate, coastal region

  • Hilti corrosion testing center Germany
    3 / 7
    Germany

    cold climate, coastal region

  • Hilti corrosion testing center Austria
    4 / 7
    Austria

    industrial site, steel works

  • Hilti corrosion testing center Mexico
    5 / 7
    Mexico

    tropical climate, coastal region

  • Hilti corrosion testing center France
    6 / 7
    France

    moderate climate, coastal region

  • Hilti corrosion testing center China
    7 / 7
    China

    tropical climate, coastal region

Special Service Arrangement Know more

CONTACT US
CONTACT US