Added to cart
Added to cart
Go to shopping cart

HOW TO DESIGN FOR THERMAL MOVEMENT

Thermal expansion design

Hilti MM modular support system for light-medium duty applications

If you’re building piping applications then it’s vital to bear in mind thermal expansion – particularly for heating applications.

This is because you will need to allow the pipes to expand and to ensure a uniform distribution of how the pipes move.

WHAT CAUSES THERMAL EXPANSION?

Thermal expansion depends on a few key factors:

  • The original length of the section of pipe
  • The coefficient of expansion
  • The temperature difference

This is usually the change in temperature between the operational temperature of the pipe and the temperature outside. So, for instance for heating applications, the operational temperature would be around 70 °C and the ambient temperature typically 20 °C.

How to calculate thermal expansion

ASK AN ENGINEER

TIPS WHEN DESIGNING FOR THERMAL EXPANSION

  • Calculate the length of expansion as a function of the length of the pipe, the pipe material and the temperature gradient.
  • Check if the displacement between the pipe axis and the upper channel surface is more than 4°. If so, you’ll need a compensation solution. Please note that application-specific requirements may affect the amount of permitted displacement.
  • Choose between natural or technical compensation, taking into account the amount of space required for each solution.

Special Service Arrangement Know more

CONTACT US
CONTACT US