On!Track Release Notes

ON!Track provides frequent releases and updates to the web and mobile software applications in order to continuously improve and add new functionality for its users. Find all the details about each software release below.

On!Track Release Notes

Version Release type  Release date Release details 
3.4 Software Release Major Feb 2020

The ON! Track 3.4 software release focuses mainly on the edit function. We have also brought up several enhancements to improve the transparency of the software and in addition, made several bug fixes to improve the performance of ON!Track.
Hilti ON Track 3.4 release highlights:

  • Multi edit: you can edit assets, commodities and consumables in bulk
  • Active Tracking: the activation of geo-location map is much faster
  • Various bug fixes: More than 15 bug fixes to improve the performance of ON!Track.
3.3 Software Release Major Oct 2019

Improvement:

In-Transit assets can now be confirmed automatically when being transferred back to their default location.

3.2.7 Mobile app Patch  Aug 2019

Improvement:

Increased the amount of barcode types supported by the new scanning technology, which allows you to accurately scan much faster, at wider angles and under different light conditions.

3.2.5 Web & Mobile app Minor release Jul 2019

Hilti ON Track 3.2.5 release highlights for all users:

- New Scanning Library: Update to a new SDK (Software Development Kit) library for improved barcode scanning via the mobile application. Ensuring verification if a scan code is registered in a customer account and fixing an issue with the number of scanned assets.

- Transfer Improvement: Making “To Location” field mandatory while performing a transfer on the Mobile app.

- NFR Update: Updating the minimum supported OS version displayed on the mobile app store and on the product info page.

- Issue Fixes: Additional minor bug fixes.

3.2 Software Release Major Mar 2019

The ON! Track 3.2 software release brings several improvements to ON!Track for the mobile, the web and active tracking. All employees are encouraged to update their mobile app to benefit from these features. We have also, made several bug fixes to improve the performance of ON!Track.

Hilti ON Track 3.2 release highlights:

  • MOBILE: Home Screen Updated
  • MOBILE: A Newly Added Request Feature
  • MOBILE: Add To Transfer Cart Updated
  • MOBILE: Edit Asset Details Updated
  • MOBILE: Add Item Barcode Scanner Updated
  • MOBILE: Image Upload Failed Messages Added
  • MOBILE: Task code Field to Transfer Added
  • WEB: Counter For Selected Assets Added
  • WEB: Automatically Email Delivery Note Added
  • WEB: Editing Stock Locations For Consumables And Impact On Archive Location Added
  • ACTIVE TRACKING: New Colum In The Grid “BLE LAST SEEN” Added
  • BUG FIXES: More than 20 bug fixes to improve the performance of ON!Track

 

Disclaimer: After the new version, has been released, all the ON!Track users should log out first and log in back to ON!Track both on the mobile and the web application to be sure the new version of ON!Track will work as it’s intended.

3.1 Software Release  Major Oct 2018 The ON! Track 3.1 software release focuses mainly on transfer updates in the mobile version of ON!Track. We have also brought up several enhancements to improve the transparency of the software and in addition, made several bug fixes to improve the performance of ON!Track.
Hilti ON Track 3.1 release highlights:
  • Transfer Queue: You can manage any pending and failed transfers in the new Transfer Queue feature. You can edit these items and either resubmit or delete them from the queue.
  • Select consumables and commodities from multiple locations: You can now control the “Quantity” and “From Location” (including the ability to select from multiple locations).
  • Transfer Error: You have now the ability to view the reasons behind a failed transfer and command actions regarding them.
  • Next Scheduled service info is now easier to access.: You can see the next scheduled service in the side panel for up to 25 services..
  • Transferring consumables/commodities: Whenever transferring commodity or consumable, user’s location is pre-populated with user’s location. In addition, you can also choose whether you want to have confirm delivery function used or not.
  • Various bug fixes: More than 20 bug fixes to improve the performance of ON!Track.
3.0 Software Release
Major May 2018

Disclaimer: After the new version, has been released, all the ON!Track users should log out first and log in back to ON!Track both on the mobile and the web application to be sure the new version of ON!Track will work as it’s intended.

Hilti ON Track 3.0 release highlights:

  • Transferring Consumables/Commodities: To improve transparency and better usability while confirming delivery on mobile the From location and the quantity are shown.
  • Request a Tool Repair: Select your tool from ON!Track and click on the “wrench button” to request a repair via Hilti Online! (Only in GPDH2 Countries!)
  • Category & ID Management: Re-design of the Asset Details section for more ease of use and transparency.
  • Alerts: We’ve re-worked how the various alerts being generated to improve and fix their reliability.
  • Service Templates: Updating service intervals on template level now updates all Assets service intervals which mapped to the service.

A more detailed overview of what features and enhancements are included in the 3.0 release can be found at the Hilti website here.

2.9 Software Release

Major

March 2018

Disclaimer: After the new version, has been released, all the ON!Track users should log out first and log in back to ON!Track both on the mobile and the web application to be sure the new version of ON!Track will work as it’s intended.

The V2.9 release brings some quintessential new features like Asset deletion at any time for admin users and changes on how you can add and manage Consumables.

Many new improvements also included such as:

  • New languages (Korean, Japanese, HK Chinese)
  • Ability to add your Hilti unique asset already to ON!Track by scanning it’s ON!Track QR code
  • Clickable hyperlinks on the Asset notes section, adjustable width of the Asset side panel
  • Re-designed Company Settings
2.8 Software Release
Major
October 2017

• Easily add and complete services from mobile: You can now easily add and complete services of your assets on the mobile app as well including uploading service attachments for it.

• View and download asset attachments on the mobile app – always have your user manuals and checklists ready.

• Add attachments to employee certificates: Certificates can be renewed, have attachments and their complete history viewable on the web.

• Employee picture: Option to upload a profile picture of every user on the web.

Watch ON!Track release highlights video

2.7 Web & Mobile app Patch July 2017 The 2.7 patch brings improvements and bug fixes on alerts, grids, reports, and more.
2.6 Web & Mobile app Major release Jun 2017

The 2.6 web and mobile patch updated the following issues:

• A complete redesign of the reporting section on the web application to make reporting faster, easier, and more efficient

• Grid views can now be saved as favorites to eliminate the recreation of frequently used views.

• The login details on the mobile app are now remembered so that users are always logged in.

• There are some enhancements and bug fixes included.

2.5.2 Web & Mobile app
Patch March 2017 The 2.5.2 patch brings several bug fixes on alerts, translations, asset grid details, and others.
2.5 Web & Mobile app Major release Mar 2017

The 2.5 web and mobile patch updated the following issues:
• Track asset ownership and responsibility securely with the revamped confirm delivery feature (including a signature field on the mobile app). 

• With the new location management concept of “location states”, manage your locations more easily by archiving completed jobsites.

• View the most recently completed services along with their attachments directly on the mobile app.

• Additional information on Hilti specific assets and data has been implemented and is viewable in the web app.

• Global searches in the web app has been improved for large customers with over 5,000 assets or locations.

• The resolution of some synchronization inconsistencies and other minor bug fixes were completed.

• Three new languages are now supported: Czech, Slovakian, and Turkish.

2.4.0.2 Web app Patch Nov 2016 The 2.4.0.2 web patch fixed the following issues:
• Errors in the check inventory and transfer reports
• Behavior of the responsible employee field during asset transfers
2.4.1 Mobile app Patch  Nov 2016 The 2.4.1 mobile patch fixed the following issues:
• Errors in the check inventory report
2.4 Web app Minor release Oct 2016 The 2.4 web release brings the following new features and enhancements:
• Finnish, Danish, and Swedish are now available
• Further improvements to the performance and search functionality have been implemented
2.4 Mobile app Minor release Oct 2016 The 2.4 mobile release brings the following new features and enhancements:
• Finnish, Danish, and Swedish are now available
• Further improvements to the performance and search functionality have been implemented
2.3.2 Web app Patch Aug 2016 With this patch important columns were brought back in the asset and location grid that were removed with the V2.3 release. The list of returned columns are:
• Fleet Cost Center, Cost Code, Extended Warranty, Fleet Organization Reference Number, Location Cost Center, Purchase Order Number, Rental Start Date, Rental Tool Claim, Template Name, Vendor
2.3.1 Mobile app Minor release Aug 2016 The mobile release from V2.3 was delayed one week and is now available as version V2.3.1.
2.3 Web & Mobile app Major release Aug 2016 Hilti ON Track version 2.3 release highlights:
• Upcoming maintenance is now announced directly within the ON!Track software so that all users are able to plan better around the availability of the system. 
• New grid functionality has been implemented to improve performance on the speed of the data loading.
• Improvements and optimizations have been made in terms of performance and search capabilities.
• The latest release documentation can be reached with a link from the ON!Track “support & info” page in the software.
• When adding an asset on the mobile it is now possible to also add asset notes, a friendly name, and an asset group.
• Restocking consumables has become easier with the ability to select and restock multiple consumable types within one transaction.
• There is a new box to highlight where the barcode scanning should take place to speed up the scanning process.

LOOKING FOR MORE INFORMATION ON ON!TRACK?