Selection of Anchor Bolt for Fixing Hoisting Beam

Posted by Katherine Wuabout 4 years ago
Selection of Anchor Bolt for Fixing Hoisting Beam

Hello
I am currently preparing BD submission for the hoisting beam. We proposed to fix it using HST3-R M16 hef2 stainless steel A4, using FOS=3, but it fails if horizontal shear force and moment are also considered. Would you help me to propose a suitable model and size that is also included in the BD reference list? Thank you so much.

anchor bolts,BD reference

1 Reply
Posted by Danielabout 4 years ago
Hilti Verified

Dear Katherine,

Thank you for your enquiry.

If the loading capacity of HST3-R M16 hef2 cannot meet your requirement, you may consider a larger size of anchor. HST3-R M20 or M24 are both included in the BD reference with the reference no. BD-AF 153.

Regards,
Daniel
Technical Engineer