On!Track Release Notes
ON!Track provides frequent releases and updates to the web and mobile software applications in order to continuously improve and add new functionality for its users. Find all the details about each software release below.
On!Track Release Notes
| Version | Release type | Release date | Release details |
|---|---|---|---|
| 3.5 Web & Mobile App | Major | Dec 2021 |
We are very excited to announce the release of PI2/2021! With this release, we are reaching an extremely important milestone of merging our Hilti ON!Track 3 and Hilti Connect mobile apps. Access for all LTS and Fleet customers: ON!Track Tool Manager features Hilti smart products Field Request Costs of Quantity Items |
| 3.4 Software Release | Major | Feb 2020 | The ON! Track 3.4 software release focuses mainly on the edit function. We have also brought up several enhancements to improve the transparency of the software and in addition, made several bug fixes to improve the performance of ON!Track.
|
| 3.3 Software Release | Major | Oct 2019 | Improvement: In-Transit assets can now be confirmed automatically when being transferred back to their default location. |
| 3.2.7 Mobile app | Patch | Aug 2019 | Improvement: Increased the amount of barcode types supported by the new scanning technology, which allows you to accurately scan much faster, at wider angles and under different light conditions. |
| 3.2.5 Web & Mobile app | Minor release | Jul 2019 | Hilti ON Track 3.2.5 release highlights for all users: - New Scanning Library: Update to a new SDK (Software Development Kit) library for improved barcode scanning via the mobile application. Ensuring verification if a scan code is registered in a customer account and fixing an issue with the number of scanned assets. - Transfer Improvement: Making “To Location” field mandatory while performing a transfer on the Mobile app. - NFR Update: Updating the minimum supported OS version displayed on the mobile app store and on the product info page. - Issue Fixes: Additional minor bug fixes. |
| 3.2 Software Release | Major | Mar 2019 | The ON! Track 3.2 software release brings several improvements to ON!Track for the mobile, the web and active tracking. All employees are encouraged to update their mobile app to benefit from these features. We have also, made several bug fixes to improve the performance of ON!Track. Hilti ON Track 3.2 release highlights:
Disclaimer: After the new version, has been released, all the ON!Track users should log out first and log in back to ON!Track both on the mobile and the web application to be sure the new version of ON!Track will work as it’s intended. |
| 3.1 Software Release | Major | Oct 2018 | The ON! Track 3.1 software release focuses mainly on transfer updates in the mobile version of ON!Track. We have also brought up several enhancements to improve the transparency of the software and in addition, made several bug fixes to improve the performance of ON!Track. Hilti ON Track 3.1 release highlights:
|
| 3.0 Software Release |
Major | May 2018 | Disclaimer: After the new version, has been released, all the ON!Track users should log out first and log in back to ON!Track both on the mobile and the web application to be sure the new version of ON!Track will work as it’s intended.
A more detailed overview of what features and enhancements are included in the 3.0 release can be found at the Hilti website here. |
2.9 Software Release |
Major |
March 2018 |
Disclaimer: After the new version, has been released, all the ON!Track users should log out first and log in back to ON!Track both on the mobile and the web application to be sure the new version of ON!Track will work as it’s intended. The V2.9 release brings some quintessential new features like Asset deletion at any time for admin users and changes on how you can add and manage Consumables. Many new improvements also included such as:
|
| 2.8 Software Release |
Major |
October 2017 |
• Easily add and complete services from mobile: You can now easily add and complete services of your assets on the mobile app as well including uploading service attachments for it. • View and download asset attachments on the mobile app – always have your user manuals and checklists ready. • Add attachments to employee certificates: Certificates can be renewed, have attachments and their complete history viewable on the web. • Employee picture: Option to upload a profile picture of every user on the web. Watch ON!Track release highlights video |
| 2.7 Web & Mobile app | Patch | July 2017 | The 2.7 patch brings improvements and bug fixes on alerts, grids, reports, and more. |
| 2.6 Web & Mobile app | Major release | Jun 2017 | The 2.6 web and mobile patch updated the following issues: • Grid views can now be saved as favorites to eliminate the recreation of frequently used views. • The login details on the mobile app are now remembered so that users are always logged in. • There are some enhancements and bug fixes included. |
| 2.5.2 Web & Mobile app |
Patch | March 2017 | The 2.5.2 patch brings several bug fixes on alerts, translations, asset grid details, and others. |
| 2.5 Web & Mobile app | Major release | Mar 2017 | The 2.5 web and mobile patch updated the following issues: • With the new location management concept of “location states”, manage your locations more easily by archiving completed jobsites. • View the most recently completed services along with their attachments directly on the mobile app. • Additional information on Hilti specific assets and data has been implemented and is viewable in the web app. • Global searches in the web app has been improved for large customers with over 5,000 assets or locations. |
| 2.4.0.2 Web app | Patch | Nov 2016 | The 2.4.0.2 web patch fixed the following issues: • Errors in the check inventory and transfer reports • Behavior of the responsible employee field during asset transfers |
| 2.4.1 Mobile app | Patch | Nov 2016 | The 2.4.1 mobile patch fixed the following issues: • Errors in the check inventory report |
| 2.4 Web app | Minor release | Oct 2016 | The 2.4 web release brings the following new features and enhancements: • Finnish, Danish, and Swedish are now available • Further improvements to the performance and search functionality have been implemented |
| 2.4 Mobile app | Minor release | Oct 2016 | The 2.4 mobile release brings the following new features and enhancements: • Finnish, Danish, and Swedish are now available • Further improvements to the performance and search functionality have been implemented |
| 2.3.2 Web app | Patch | Aug 2016 | With this patch important columns were brought back in the asset and location grid that were removed with the V2.3 release. The list of returned columns are: • Fleet Cost Center, Cost Code, Extended Warranty, Fleet Organization Reference Number, Location Cost Center, Purchase Order Number, Rental Start Date, Rental Tool Claim, Template Name, Vendor |
| 2.3.1 Mobile app | Minor release | Aug 2016 | The mobile release from V2.3 was delayed one week and is now available as version V2.3.1. |
| 2.3 Web & Mobile app | Major release | Aug 2016 | Hilti ON Track version 2.3 release highlights: • Upcoming maintenance is now announced directly within the ON!Track software so that all users are able to plan better around the availability of the system. • New grid functionality has been implemented to improve performance on the speed of the data loading. • Improvements and optimizations have been made in terms of performance and search capabilities. • The latest release documentation can be reached with a link from the ON!Track “support & info” page in the software. • When adding an asset on the mobile it is now possible to also add asset notes, a friendly name, and an asset group. • Restocking consumables has become easier with the ability to select and restock multiple consumable types within one transaction. • There is a new box to highlight where the barcode scanning should take place to speed up the scanning process. |
ON!Track Web Manual
ON!Track Mobile Manual